Description - Facility Explorer - Metasys - LIT-1900869 - Gateway/Router - MAP Gateway - 5.0

Mobile Access Portal Gateway Catalog Page

Brand
Facility Explorer
Metasys
Product name
MAP Gateway
Document type
Catalog Page
Document number
LIT-1900869
Version
5.0
Revision date
2018-12-17
Language
English

The Mobile Access Portal (MAP) Gateway is a pocket-sized web server that provides a wireless mobile user interface to Smart Equipment Rooftop Units (RTUs). The mobile user interface can be displayed in the browser of a phone, tablet, or computer.

The MAP Gateway ships from the factory with a base set of features that allow users to access, view, edit, and override key information from all devices connected on a common BACnet Token Passing (TP) field bus. The wireless connection on the MAP Gateway allows users to be up to 31m (100 ft line of sight) away indoors and up to 91 m (300 ft line of sight) away outdoors. The MAP Gateway can also be permanently mounted, powered with an optional separate power supply and connected to an Ethernet access point for use as remote connection to a TP field bus of devices.

MAP Gateways ship from the factory with version 5.0x firmware, MAP Gateway units already in the field with version 3.0x firmware or later can be upgraded to Release 5.0 to provide a complete set of Commissioning and Wiring Validation functions targeted for use by electricians, commissioning contractors, and technicians.

The Release 5.0 upgrade can be acquired from Johnson Controls internal portal pages or Offering's Catalog on HVAC Navigator. These updates are complemented by a set of targeted videos that are available using the following link https://jcpublic.kzoplatform.com/containers/957891534378768109.

The YK MAP Gateway cannot be used on anything other than Smart Equipment Rooftops. You must have the latest version of MAP to view latest features in Smart Equipment.

The MAP Gateway user interface is accessed either over Wi-Fi or an existing Ethernet network on site.

Figure 1. Mobile Access Portal Gateway