Connecting the VAV Box Balancing Sensor - Facility Explorer - Part No. 24-10211-10 - Field Device - VAV: Variable Air Volume Controller

Handheld VAV Box Balancing Sensor Installation Instructions

Product
Variable Air Volume > Variable Air Volume Controls > VAV: Variable Air Volume Controller
Document number
Part No. 24-10211-10
Document revision
B
Revision date
2019-03-22

About this task

Observe the following guidelines and procedures when connecting the VAV Box Balancing Sensor to your system.

Procedure

  1. Connect one male end of the supplied cable to the VAV Box Balancing Sensor.
  2. Connect the other end of the cable to the controller or network sensor.
    Important:

    The VAV Box Balancing Sensor has a dedicated MS/TP bus address of 198. Only one VAV Box Balancing Sensor can be connected to the MS/TP bus per physical trunk on the system.