Repair information - Facility Explorer - Part No. 24-10211-10 - Field Device - VAV: Variable Air Volume Controller

Handheld VAV Box Balancing Sensor Installation Instructions

Product
Variable Air Volume > Variable Air Volume Controls > VAV: Variable Air Volume Controller
Document type
Installation Guide
Document number
Part No. 24-10211-10
Document revision
B
Revision date
2019-03-22

Do not open the VAV Box Balancing Sensor housing. The VAV Box Balancing Sensor has no user-serviceable parts inside. The VAV Box Balancing Sensor requires no periodic field maintenance.

If the VAV Box Balancing Sensor fails to operate within its specifications, replace the unit. For a replacement sensor, contact the nearest Johnson Controls® representative.