Using the VAV Box Balancing Sensor - Facility Explorer - Part No. 24-10211-10 - Field Device - VAV: Variable Air Volume Controller

Handheld VAV Box Balancing Sensor Installation Instructions

Product
Variable Air Volume > Variable Air Volume Controls > VAV: Variable Air Volume Controller
Document number
Part No. 24-10211-10
Document revision
B
Revision date
2019-03-22

Once the VAV Box Balancing Sensor is physically connected to the VAV controller’s bus, you can use the sensor to balance the VAV box.