Parts included - Facility Explorer - Part No. 24-10211-10 - Field Device - VAV: Variable Air Volume Controller

Handheld VAV Box Balancing Sensor Installation Instructions

Product
Variable Air Volume > Variable Air Volume Controls > VAV: Variable Air Volume Controller
Document number
Part No. 24-10211-10
Document revision
B
Revision date
2019-03-22

Included in this package are the following items:

  • One handheld VAV Box Balancing Sensor
  • One 5 ft retractable cable
  • One padded carrying case
  • One set of installation instructions