Devices in the BACnet/SC topology - Facility Explorer - LIT-12014410 - BACnet Secure Connect BACnet Datalink - Metasys SNC Series Network Control Engine

Facility Explorer BACnet/SC Commissioning Guide

Product
Network and Communications > BACnet > BACnet Secure Connect BACnet Datalink
Document type
Commissioning Guide
Document number
LIT-12014410
Revision date
2024-05-21
Product status
Active
This table describes Facility Explorer devices and their role in the BACnet/SC topology and maximum supported connections. Dual mode refers to the ability to maintain both BACnet/SC and BACnet/IP connections simultaneously.
Table 1. Facility Explorer BACnet/SC device information
Facility Explorer device Can serve as hub Maximum hub connections Supports dual mode
FX90 Supervisory Controller Yes 1,000 Yes
FX80 Supervisory Controller Yes 250 Yes
F4-SNC Supervisory Controller: all models Yes 50 Yes

F4-CGE04060-0

F4-CGE09090-0

F4-CGE09090-0H

F4-CVE03050-0P

FX-PCA4911-0

FX-PCV1930-0

No. These devices are only nodes, as they cannot act as primary or failover hub. n/a No