Discovering the new station in BACnet network - Facility Explorer - LIT-12014410 - BACnet Secure Connect BACnet Datalink - Metasys SNC Series Network Control Engine

Facility Explorer BACnet/SC Commissioning Guide

Product
Network and Communications > BACnet > BACnet Secure Connect BACnet Datalink
Document type
Commissioning Guide
Document number
LIT-12014410
Revision date
2024-05-21
Product status
Active

Procedure

  1. Navigate to Drivers > BACnetNetwork.
  2. Click Discover.
  3. Click Ok. All SC stations can now be transferred to the database.