Creating a client certificate in the Platform Certificate Manager and assigning it to Node Station - Facility Explorer - LIT-12014410 - BACnet Secure Connect BACnet Datalink - Metasys SNC Series Network Control Engine
Facility Explorer BACnet/SC Commissioning Guide
- Product
- Network and Communications > BACnet > BACnet Secure Connect BACnet Datalink
- Document type
- Commissioning Guide
- Document number
- LIT-12014410
- Revision date
- 2024-05-21
- Product status
- Active
Procedure
-
In Workbench, navigate to the platform hosting the new station.
-
Click Certificate Management.
-
To create a new client certificate, click New. Assign an
alias name, common name, and country code with two characters.
-
Under Certificate Usage, select
Client. Match the details of the CA certificate for
the site.
-
Generate a Cert Request for Client Cert. Save this in the same folder on the
local hard drive as the CA.
-
Under Tools, click Certificate Signer
Tool.
-
In the Select a certificate signing request to sign
field, select the client CSR.
-
In the CA Alias entry, select the CA.
-
Enter the password for the CA.
-
Click Ok.
-
Import the signed Code Signing Cert into User Key Store. The alias turns green.