Confirming the primary hub node is successfully connected to the new station - Facility Explorer - LIT-12014410 - BACnet Secure Connect BACnet Datalink - Metasys SNC Series Network Control Engine

Facility Explorer BACnet/SC Commissioning Guide

Product
Network and Communications > BACnet > BACnet Secure Connect BACnet Datalink
Document number
LIT-12014410
Revision date
2024-05-21
Product status
Active

Procedure

  1. In the primary hub station, navigate to Drivers > BacnetNetwork > Bacnet Comm > ScHubPort > Link > HubFunction > Connections.
  2. If the connections are successful, the connection appears as ConnectionX where X is the connection number in the order that connections were made.
  3. In each connection, confirm that State and Sub State are connected.
    Note: Do no rename connections. When you change display names of connections, use Set Display Name.