Importing signing certificates and operational certificates in JCT - Facility Explorer - LIT-12014410 - BACnet Secure Connect BACnet Datalink - Metasys SNC Series Network Control Engine

Facility Explorer BACnet/SC Commissioning Guide

Product
Network and Communications > BACnet > BACnet Secure Connect BACnet Datalink
Document number
LIT-12014410
Revision date
2024-05-21
Product status
Active

Procedure

  1. In JCT, select the devices with the check boxes on the left.
  2. From the ACTIONS list, click Importing Signing Certificate.
  3. In the Import Signing Certificate window, click Choose File to browse for the .pem file.
  4. Click the check box to confirm this file is from a trusted source. Click IMPORT AND APPLY.
  5. Use the check boxes on the left to select devices.
  6. Click Import Operational Certificate(s) in the upper right.
  7. Import the .zip file created in the previous section. This .zip file contains all of the signed operational certificates of the F4-SNC Supervisory Controllers and the field controllers.
  8. Click the check box to confirm this file is from a trusted source. Click IMPORT AND APPLY. The status icons of the devices turn green to signify the import is successful.