Importing a code signing certificate into the User Key Store - Facility Explorer - LIT-12014410 - BACnet Secure Connect BACnet Datalink - Metasys SNC Series Network Control Engine
Facility Explorer BACnet/SC Commissioning Guide
- Product
- Network and Communications > BACnet > BACnet Secure Connect BACnet Datalink
- Document number
- LIT-12014410
- Revision date
- 2024-05-21
- Product status
- Active
Procedure
-
In FX Workbench, from the Tools menu, click
Certificate Signer Tool.
-
In the Certificate Signing window, click the folder icon
beside Select a certificate signing request to sign and
browse for the
.csr file. Click
Open.
-
From the CA Alias list, select the CA you want to sign
the certificate with.
-
In the CA Password field, enter the password for the
CA.
-
Click OK. The file saves as a
.pem
file.
-
In the User Key Store, click
Import. Select the
.pem file. Click
Open.
-
In the Private Key Password, enter the code signing cert
password. The alias turns green.