Generating CSRs from Workbench - Facility Explorer - LIT-12014410 - BACnet Secure Connect BACnet Datalink - Metasys SNC Series Network Control Engine

Facility Explorer BACnet/SC Commissioning Guide

Product
Network and Communications > BACnet > BACnet Secure Connect BACnet Datalink
Document number
LIT-12014410
Revision date
2024-05-21
Product status
Active

Procedure

  1. In FX Workbench, from the Tools menu, click Certificate Signer Multiple Selection Tool. This allows you to sign multiple certificates at one time.
  2. In the Select Certificate Signing Request(s) window, from the Files of type list, click All Files. Browse for the .pem files. Click Open.
  3. From the CA Alias list, select the CA. Enter the CA password.
  4. Click Generate. Browse to the same folder as the original CA. Click Choose. Click OK on the confirmation dialog box.
  5. Zip the newly signed certificates into a .zip file. Save the .zip file in the same folder on your local hard drive as the CA.