Exporting CSRs in JCT - Facility Explorer - LIT-12014410 - BACnet Secure Connect BACnet Datalink - Metasys SNC Series Network Control Engine
Facility Explorer BACnet/SC Commissioning Guide
- Product
- Network and Communications > BACnet > BACnet Secure Connect BACnet Datalink
- Document type
- Commissioning Guide
- Document number
- LIT-12014410
- Revision date
- 2024-05-21
- Product status
- Active
Procedure
-
Log on to JCT at https://localhost/UIOffline/#/.
-
In the Device Connection window, enter the hostname for
the SNC Supervisory Controller in the Hostname / IP
Address field. Enter the username and password of the SNC
Supervisory Controller. Click LOG IN.
-
In the Select Archive window, select the archive from
the list. Click SELECT ARCHIVE. You may be prompted to do
this log on again.
-
Open the BACnet/SC Management page. You can also find
the BACnet/SC Management page in the top right menu under
Network Security.
-
To see all devices, select FILTER. From the
Network Device list, click All
Devices.
-
Use the check boxes on the left of the screen to select the devices.
-
From the ACTIONS list, click Request
Certificate(s). Enter the information for the certificate you
want to create. The required fields are Email Address,
Organization, Organizational
Unit, Country. Click
REQUEST.
-
In the Request Certificate(s) window, click
DOWNLOAD CSR(S). The certificate signing request
saves as a
.zip
file. Extract the files from the
.zip
file into the same folder as your CA on your local
hard drive.