BACnet/SC network configuration - Facility Explorer - LIT-12014410 - BACnet Secure Connect BACnet Datalink - Metasys SNC Series Network Control Engine

Facility Explorer BACnet/SC Commissioning Guide

Product
Network and Communications > BACnet > BACnet Secure Connect BACnet Datalink
Document number
LIT-12014410
Revision date
2024-05-21
Product status
Active
This section describes a BACnet/SC network with the following configuration:
  • The FX90 Supervisory Controller as the primary hub
  • The F4-SNC Supervisory Controller as the failover hub
  • Facility Explorer IP equipment controllers as nodes

For an example network scenario, see Figure 2 and Figure 3.