Creating a server certificate to assign to SC Hub - Facility Explorer - LIT-12014410 - BACnet Secure Connect BACnet Datalink - Metasys SNC Series Network Control Engine
Facility Explorer BACnet/SC Commissioning Guide
- Product
- Network and Communications > BACnet > BACnet Secure Connect BACnet Datalink
- Document number
- LIT-12014410
- Revision date
- 2024-05-21
- Product status
- Active
Procedure
-
In FX Workbench, open a station connection to an FX90
platform.
-
Navigate to .
-
To create a new server certificate, click New. Assign an
alias name, common name, and country code with two characters.
-
Under Certificate Usage, select
Server.
-
Generate a cert request for the server certificate. Save this in the same
folder on your local hard drive as the CA.
-
Under Tools, click Certificate Signer
Tool.
-
In the Select a certificate signing request to sign
entry, select the server certificate CSR.
-
In the CA Alias entry, select the CA.
-
Enter the password for the CA.
-
Click Ok.
-
Import the code signing certificate into User Key Store. The alias turns
green.