Configuring the web service of your station - Facility Explorer - LIT-12014410 - BACnet Secure Connect BACnet Datalink - Metasys SNC Series Network Control Engine
Facility Explorer BACnet/SC Commissioning Guide
- Product
- Network and Communications > BACnet > BACnet Secure Connect BACnet Datalink
- Document number
- LIT-12014410
- Revision date
- 2024-05-21
- Product status
- Active
Procedure
-
Navigate to .
-
From the Https Min Protocol list, select
TLSv1.3.
-
In the Https Port field, enter the port number. The
default port number is 443.
-
Go to Main Https Cert. Select the server certificate
that you previously created, signed, and imported.
-
Click Save.
-
Navigate to . From the Enabled list, select
true.