Configuring SC network settings for FX controllers - Facility Explorer - LIT-12014410 - BACnet Secure Connect BACnet Datalink - Metasys SNC Series Network Control Engine

Facility Explorer BACnet/SC Commissioning Guide

Product
Network and Communications > BACnet > BACnet Secure Connect BACnet Datalink
Document number
LIT-12014410
Revision date
2024-05-21
Product status
Active

About this task

Complete the following procedure in UIOffline connected to the F4-SNC network.

Procedure

  1. In the Devices list, select the SNC device. Change the mode to Dual SC and IP Mode.
  2. Select the SNC device check box.
  3. Click Actions > Set BACnet IP Communication Mode.
  4. Set all other node devices to Ethernet IP Only Mode.
  5. Navigate to the Settings tab.
  6. In the Secure Port Number field, enter the secure port number to match the SC network number in the Workbench station.
  7. In the SC Primary Hub URI field, enter the SC primary hub URI in the following format: wss://<IP address of the FX90>:<https port number>/hub
    Note: You can find the https port number in Config > Services > WebService.
  8. In the SC Failover Hub URI field, enter the SC failover hub URI in the following format: wss://<IP address of the SNC>:<secure port number>/
  9. Click SAVE.
  10. Select all the node devices checkboxes. From the Actions list, select Set BACnet IP Communication Mode.
  11. In the Set BACnet IP Communication Mode window, select Secure Connect Only Mode. Click APPLY.
  12. Keep the SNC in Dual SC and IP Mode until you confirm all connections.