Adding and configuring an ScHubPort into the BACnet network - Facility Explorer - LIT-12014410 - BACnet Secure Connect BACnet Datalink - Metasys SNC Series Network Control Engine

Facility Explorer BACnet/SC Commissioning Guide

Product
Network and Communications > BACnet > BACnet Secure Connect BACnet Datalink
Document number
LIT-12014410
Revision date
2024-05-21
Product status
Active

Procedure

  1. Navigate to Station > Config > Drivers > Bacnet Comm > Network.
  2. Drag and drop an ScHubPort from the Palette window at the bottom left to Network object in the navigation tree.
  3. In the Property Sheet, under ScHubPort, set a Network Number.
  4. Navigate to ScHubPort > Link > Credentials.
  5. In the Operational Certificate field, select the signed server certificate.
  6. In the Issuer Certificate field, under Issuer Certificate 1, select the certificate authority certificate.
  7. Go to HubFunction. From the Enabled list, select true.
  8. Go to Hub Connector > Primary Connection and ensure the Hub Uri Address field is set to localhost and the Hub Uri Path is set to hub. The station connects to itself as the primary hub.
  9. Click Save.
  10. Right click HubFunction > Actions > Add Sc user.
  11. Leave ScHubPort disabled at this time.
    Note: The entry at Hub Connector > Primary Connection > Hub Uri Address must read localhost. The station connects to itself as the primary hub.