Web-based user interface - Facility Explorer - LIT-12014354 - FX-SC9BASE-0 - FX-SC9BASE-0E - FX90 Supervisory Controller - 14.13

FX90 Supervisory Controller Product Bulletin

Product
Controls > Supervisory Controls > FX90 Supervisory Controller
Document number
LIT-12014354
Version
14.13
Revision date
2024-10-31
Product status
Active

The FX Supervisory Controller’s web-based user interface (Web UI) provides system-wide monitoring and control capability through a web browser. The Web UI capability is embedded in every FX Supervisory Controller, allowing users to access the system using a web browser over an Ethernet LAN or internet connection.

When you create your Web UI pages, you can choose from a full library of colorful, 3D graphical symbols including the following symbols:
  • HVAC equipment
  • Duct work
  • Coils
  • Piping
  • Control devices, for example, dampers or valves
  • Widgets, for example, buttons, tables, or hyperlinks

In addition, you can import your own digital images, for example, a floor-plan JPEG, and incorporate them into your Web UI.

The FX90 features modernized 3D graphics that have the same look and feel on any tablet, laptop, mobile phone device, without the need to create separate graphics for different device platforms. You can view devices, points, schedules, alarms, and graphics with the convenience of a wireless handheld device. You can also acknowledge alarms, command points, and modify schedules. The user interface updates dynamically, so that when changes are made to the FX Supervisor configuration, these changes automatically appear.

Figure 1. Mobile device Web UI

Figure 2. Full-sized Web UI