Scheduling - Facility Explorer - LIT-12014354 - FX-SC9BASE-0 - FX-SC9BASE-0E - FX90 Supervisory Controller - 14.13

FX90 Supervisory Controller Product Bulletin

Product
Controls > Supervisory Controls > FX90 Supervisory Controller
Document number
LIT-12014354
Version
14.13
Revision date
2024-10-31
Product status
Active
You can configure the FX90 Supervisory Controller to automate various functions in a facility based on a time schedule:
  • Determine the expected occupancy periods
  • Start or stop HVAC equipment
  • Turn lights on and off

You can link any writable point in the FX90 Supervisory Controller system database to a schedule. The scheduler interface provides a visually intuitive method for you to configure the daily, weekly, and exception or holiday schedules.

Figure 1. Scheduler