Ethernet wiring - Facility Explorer - LIT-12014353 - FX-SC9BASE-0 - FX90 Supervisory Controller - 14.x

FX90 Supervisory Controller Installation Guide

Product
Controls > Supervisory Controls > FX90 Supervisory Controller
Document type
Installation Guide
Document number
LIT-12014353
Version
14.x
Revision date
2024-03-18
Product status
Active

Two RJ-45 10/100/1000-Mbit Ethernet connectors are labeled PRI (LAN1) for primary, and SEC (LAN2) for secondary. Use a standard Ethernet patch cable to an Ethernet switch.

The factory-default IP address for PRI is 192.168.1.140 . The default subnet mask is 255.255.255.0. By default, the SEC (LAN2) port is disabled.