Communications wiring - Facility Explorer - LIT-12014353 - FX-SC9BASE-0 - FX90 Supervisory Controller - 14.x

FX90 Supervisory Controller Installation Guide

Product
Controls > Supervisory Controls > FX90 Supervisory Controller
Document number
LIT-12014353
Version
14.x
Revision date
2024-03-18
Product status
Active
Figure 1. Communications ports on the FX90 Supervisory Controller

Table 1. Communications ports on the FX90 Supervisory Controller

Callout

Description

1 Ground
2 24 V power input
3 RS-485 ports and bias switches
4 Ethernet port, 10/100/1000-Mbit, RJ-45: Pri
5 Ethernet port, 10/100/1000-Mbit, RJ-45: Sec