Turning on and performing an initial checkout - Facility Explorer - LIT-12014353 - FX-SC9BASE-0 - FX90 Supervisory Controller - 14.x
FX90 Supervisory Controller Installation Guide
- Product
- Controls > Supervisory Controls > FX90 Supervisory Controller
- Document number
- LIT-12014353
- Version
- 14.x
- Revision date
- 2024-03-18
- Product status
- Active
Procedure
-
Apply power. To do this, perform one of the following options:
- Insert the 2-position 24 V
power connector plug.
- Insert the barrel plug of the
wall-mount AC adapter (FX-SC8XPS-0).
-
Check the STAT (Status) and BEAT (Heartbeat) LEDs. When power is
applied, the green STAT LED flashes. This LED indicates that the system
works, with power applied. During startup, the BEAT LED may blink at 1 Hz
with a 90/10 percent on/off duty cycle. When startup completes, the platform
daemon starts, and the normal 1 Hz flash at 50/50 percent on/off duty cycle of
the BEAT LED returns.