Remove or replace the microSD flash memory card - Facility Explorer - LIT-12014353 - FX-SC9BASE-0 - FX90 Supervisory Controller - 14.x

FX90 Supervisory Controller Installation Guide

Product
Controls > Supervisory Controls > FX90 Supervisory Controller
Document number
LIT-12014353
Version
14.x
Revision date
2024-03-18
Product status
Active
Figure 1. MicroSD card location in the controller

Callout

Description

1

Card carrier inside the controller

2

MicroSD card to insert or remove from the card carrier

3

Access shutter for the microSD card. Slide to open or close

Important: Disconnect all power to the controller before you remove or insert the microSD card. Otherwise, equipment damage is likely to occur.
Note: When you remove the microSD card, you must lightly press on the installed microSD card shutter to release it. Then carefully remove the card from the card carrier. When you replace a microSD card, place the card in the card carrier, and push the card carrier in the access shutter until it clicks.
Note: Data on the microSD card is encrypted by a special system password stored in the controller base. If you swap in a card from a previously configured unit, you must re-enter this same passphrase using a serial connection to the unit’s debug port.
Note: Third-party microSD cards are not supported.