Figure 1. MicroSD card location in the controller

Callout |
Description |
---|---|
1 |
Card carrier inside the controller |
2 |
MicroSD card to insert or remove from the card carrier |
3 |
Access shutter for the microSD card. Slide to open or close |
Important: Disconnect all power to the controller before you remove or insert the
microSD card. Otherwise, equipment damage is likely to occur.
Note: When you remove the microSD card, you must lightly press on the installed microSD card shutter
to release it. Then carefully remove the card from the card carrier. When you
replace a microSD card, place the card in the card carrier, and push the card
carrier in the access shutter until it clicks.
Note: Data on the microSD card is encrypted by a special system password stored in the controller
base. If you swap in a card from a previously configured unit, you must re-enter
this same passphrase using a serial connection to the unit’s debug port.
Note: Third-party microSD cards are not supported.