DIN rail mounting - Facility Explorer - LIT-12014353 - FX-SC9BASE-0 - FX90 Supervisory Controller - 14.x
FX90 Supervisory Controller Installation Guide
- Product
- Controls > Supervisory Controls > FX90 Supervisory Controller
- Document number
- LIT-12014353
- Version
- 14.x
- Revision date
- 2024-03-18
- Product status
- Active
Procedure
-
Pull the FX90 Supervisory Controller's locking clip down.
Figure 1. Fastening to the rail
-
Tilt the module to hook over the DIN rail.
-
Push down and in on the unit. This fastens it to the rail.
-
Slide the module firmly into the FX90 Supervisory Controller's connector, or
existing option module, to seat.
-
Mount any option card module onto the DIN rail in the same way.
Figure 2. Slide module into FX90 Supervisory Controller's connector
-
Slide the module firmly into the FX90 Supervisory Controller's connector to
seat. Repeat for other modules as needed. Four is the maximum number of modules.
-
Secure both ends of the final assembly with DIN rail end-clips provided by the
DIN rail vendor.