LEDs - Facility Explorer - LIT-12014353 - FX-SC9BASE-0 - FX90 Supervisory Controller - 14.x

FX90 Supervisory Controller Installation Guide

Product
Controls > Supervisory Controls > FX90 Supervisory Controller
Document number
LIT-12014353
Version
14.x
Revision date
2024-03-18
Product status
Active

The FX90 Supervisory Controller features a number of status LEDs.

Figure 1. LEDs and descriptions
Callout Label Color Description
1 RS-485 A - COM1 Yellow Transmit (TX)
Green Receive (RX)
2 RS-485 B - COM2 Yellow Transmit (TX)
Green Receive (RX)
3 SHUTDOWN Impressed  
4 PRI Yellow Primary Ethernet: LAN1. Activity
Green Primary Ethernet: LAN1. Link
5 SEC Yellow Secondary Ethernet: LAN2. Activity
Green Secondary Ethernet: LAN2. Link
6 BEAT Yellow Heartbeat, normally 1 Hz 50% duty cycle
7 STAT Green Remains lit when controller is on

If the BEAT LED stays on constantly, does not light, or blinks very fast, have your ABCS Distributor contact the FSC or your appropriate technical support group.

Important: The 1 Hz, 90/10 percent on/off BEAT flash at startup also occurs during other critical operations, such as a firmware upgrade to the controller or any attached modules. To be safe, do not remove power from the controller while its BEAT LED flashes with a 90/10 percent on/off duty cycle. Wait for the normal 50/50 percent flash to return before you remove power.