Editing a wireless network - Facility Explorer - LIT-12012339 - FX-SC8BASE-0 - FX-SC8BASE-700 - Bulb controller - FX80 WiFi Supervisory Controller

FX80 WiFi Technical Bulletin

Product
Controls > Supervisory Controls > FX80 WiFi Supervisory Controller
Document number
LIT-12012339
Revision date
2019-03-22

About this task

In the Client mode configuration, you can edit connection properties for a previously accessed wireless network listed in the Network Database table.

To perform this task, you must set the WiFi Selector Switch to the CLT position. Also, make sure the connection is a previously configured WiFi network

Procedure

  1. In the WiFi Configuration view, select the Client Mode tab.
  2. Select a network listed in the Network Database pane and click Edit.
  3. In the Edit a Wireless Network dialog box, modify the values as needed.
    Note: The Show Password check box is activated once you edit the current Network Key value.