WiFi specifications - Facility Explorer - LIT-12012339 - Wireless Device - ZFR: Wireless Field Bus System

FX80 WiFi Technical Bulletin

Brand
Facility Explorer
Product name
ZFR: Wireless Field Bus System
Document type
Technical Bulletin
Document number
LIT-12012339
Revision date
2019-03-22
Language
English

You can enable and configure the WiFi feature to attach as a Client to an already established IEEE 802.11 Access Point and network, or configured as an Access Point to establish a new network.

The WiFi feature of the FX80 controller has the following features:
  • Supports IEEE 802.11a/b/g/n networks
  • Provides a configurable radio (OFF, ACC, CLT)
  • Supports WPA-PSK, WPA2-PSK security
  • Supports 2.4 or 5 GHz frequencies
  • Provides a single coax mount dual band 2.4/5 GHz antenna. Remote antenna location is possible using an extension cable.