WiFi configuration view - Facility Explorer - LIT-12012339 - FX-SC8BASE-0 - FX-SC8BASE-700 - Bulb controller - FX80 WiFi Supervisory Controller

FX80 WiFi Technical Bulletin

Product
Controls > Supervisory Controls > FX80 WiFi Supervisory Controller
Document number
LIT-12012339
Revision date
2019-03-22

The WiFi Configuration view in FX Workbench is the main view for configuring WiFi communications for an FX80 Supervisory Controller. The view includes tabs for configuring the FX80 Supervisory Controller to run in both Client mode and Access Point mode. However, the unit cannot perform in both modes at the same time.