State properties - Facility Explorer - LIT-12012339 - FX-SC8BASE-0 - FX-SC8BASE-700 - Bulb controller - FX80 WiFi Supervisory Controller

FX80 WiFi Technical Bulletin

Product
Controls > Supervisory Controls > FX80 WiFi Supervisory Controller
Document number
LIT-12012339
Revision date
2019-03-22

WiFi State properties appear in the upper portion of the view.

Table 1. State properties

Property

Value

Description

WiFi Enabled

true, false (default)

Selecting true enables WiFi functionality.

Note: The WiFi Enabled setting in the WiFi Configuration view is ignored when the unit’s WiFi Selector Switch is in the OFF (center) position.

WiFi Switch Position

Access Point, Off, Station

Indicates the current position of the WiFi Selector Switch on the unit. Read-only value.

ACC (left position) - Access Point

CLT (right position) - Station

OFF (center position) turns the WiFi subsystem completely off.