WiFi State properties appear in the upper portion of the view.
|
Property |
Value |
Description |
|---|---|---|
|
WiFi Enabled |
true, false (default) |
Selecting true enables WiFi functionality. Note: The WiFi Enabled setting in the WiFi Configuration view is ignored when the unit’s WiFi
Selector Switch is in the OFF (center)
position.
|
|
WiFi Switch Position |
Access Point, Off, Station |
Indicates the current position of the WiFi Selector Switch on the unit. Read-only value. ACC (left position) - Access Point CLT (right position) - Station OFF (center position) turns the WiFi subsystem completely off. |