Supported WiFi configurations - Facility Explorer - LIT-12012339 - FX-SC8BASE-0 - FX-SC8BASE-700 - Bulb controller - FX80 WiFi Supervisory Controller

FX80 WiFi Technical Bulletin

Product
Controls > Supervisory Controls > FX80 WiFi Supervisory Controller
Document type
Technical Bulletin
Document number
LIT-12012339
Revision date
22/03/2019

WiFi Client and Access Point modes add support for a number of new network configurations. Supported network configurations are described in the following sections.

Note: Although other network configurations may exist, the network configuration are not necessarily supported.

The FX80 controller does not support IP routing between any combination of Ethernet and WiFi ports. For example, the controller does not forward IP packets from LAN1 to LAN2, LAN1 to WiFi, WiFi to LAN2. If an installation requires IP routing between WiFi and Ethernet ports, you may configure the controller using standard IT networking infrastructure components.

In the following figures, different networks are represented by thick gray lines. The FX80 controller does not route traffic between different networks. Data may be shared at the application level.