Client mode tab - Facility Explorer - LIT-12012339 - FX-SC8BASE-0 - FX-SC8BASE-700 - Bulb controller - FX80 WiFi Supervisory Controller

FX80 WiFi Technical Bulletin

Product
Controls > Supervisory Controls > FX80 WiFi Supervisory Controller
Document number
LIT-12012339
Revision date
2019-03-22
Figure 1. WiFi configuration, Client Mode tab

Properties listed in the following table appear in the Wireless State pane of the Client Mode tab in the WiFi Configuration view.

Table 1. Wireless state configuration properties

Property

Value

Description

WiFi Attach State

disconnected, connected

Read-only value

Client Adapter

tiw_sta[n]

Read-only value. Client Adapter name appended with number 0 through the maximum number of clients configured for the Access Point.

For example: tiw_sta0, tiw_sta1, tiw_sta2

Client address

00:00:00:00:0-0:0

MAC address of the client device. Format is six HEX addresses separated by a colon (for example, 08:00:69:E2:01:FE).

Client address via DHCP

unknown

Read-only value

Access Point

unknown, last access point

Read-only value. Unknown indicates the unit has never connected to an access point. Otherwise, the last access point the unit connected to appears.

Default Gateway Switching

enabled, disabled

When enabled (checked), the system uses the gateway provided by the Access Point.

Important: When you connect to a third party Access Point, the gateway changes to reflect what is provided by the Access Point configuration. This connection conflicts with your wired LAN settings. This situation does not occur when connecting to a FX80 Access Point. When disabled (not checked), keep the gateway as assigned in TCP/IP Configuration view.

Once the WiFi Selector Switch on the unit is in the CLT position, setting the WiFi Enabled property to true activates the Discover button.

Table 2. Discovered networks

Property

Description

Discover

Scans for WiFi signals and displays a list of discovered networks.

Add

Opens the Add dialog box and allows you to configure connection properties for the selected network.

The Network Database section contains a list of added WiFi networks.

Table 3. Network database

Property

Description

Connect

Appears inactive (dimmed) until you select a network to connect to.

Disconnect

Appears inactive (dimmed) until the unit is currently connected to an access point.

Edit

Appears inactive (dimmed) until you select a network. Allows you to change configured connection priority and access point passkey.

New

Configure access point properties and add the new network to the Network Database table.

Remove

Inactive (dimmed) until you select a network to delete.