Access point - Facility Explorer - LIT-12012339 - FX-SC8BASE-0 - FX-SC8BASE-700 - Bulb controller - FX80 WiFi Supervisory Controller

FX80 WiFi Technical Bulletin

Product
Controls > Supervisory Controls > FX80 WiFi Supervisory Controller
Document number
LIT-12012339
Revision date
2019-03-22

In a wireless local area network (WLAN), a wireless Access Point is a hardware device, such as the FX80, that allows wireless devices to connect to a wired network using WiFi, or related standards. Access Points feature radio transmitters and antennae, which facilitate connectivity between devices and the Internet or a network.