Totalization - Facility Explorer - LIT-12012250 - Supervisory Device - FX80 Supervisory Controller

FX80 Supervisory Controller Product Bulletin

Product
Controls > Supervisory Controls > FX80 Supervisory Controller
Document type
Product Bulletin
Document number
LIT-12012250
Revision date
2024-11-28

The Totalization feature enables the FX Supervisory Controller to accumulate data over a period of time. You can add a totalization extension to any data point in the FX Supervisory Controller system database to summarize runtime, accumulate change of state counts, or summarize dynamic analog data. Totalized data is presented in a sortable table, and you can export it in a TXT, PDF, or CSV file format.