Histories - Facility Explorer - LIT-12012250 - Supervisory Device - FX80 Supervisory Controller

FX80 Supervisory Controller Product Bulletin

Product
Controls > Supervisory Controls > FX80 Supervisory Controller
Document type
Product Bulletin
Document number
LIT-12012250
Revision date
2021-11-03

The Histories feature collects, stores, and displays pertinent system data for analysis, such as control performance indication, energy consumption, and system troubleshooting. You can configure the FX80 controller to create a history on any data point in its system database. Histories are presented either graphically or in a sortable table, and you can export the data in a TXT, PDF, or CSV format.

Figure 1. Histories