Energy management - Facility Explorer - LIT-12012250 - Supervisory Device - FX80 Supervisory Controller

FX80 Supervisory Controller Product Bulletin

Product
Controls > Supervisory Controls > FX80 Supervisory Controller
Document type
Product Bulletin
Document number
LIT-12012250
Revision date
2021-11-03
The FX80 controller features several energy management functions, which you can enable and configure, including the following:
  • Electrical demand limiting/load shedding
  • Optimized start/stop
  • Free cooling determination