Customized control logic - Facility Explorer - LIT-12012250 - Supervisory Device - FX80 Supervisory Controller

FX80 Supervisory Controller Product Bulletin

Product
Controls > Supervisory Controls > FX80 Supervisory Controller
Document type
Product Bulletin
Document number
LIT-12012250
Revision date
2021-11-03
The FX80 controller includes a library of control logic modules that you can enable, configure, and link together to create your own customized control routines. Some examples of the available control logic modules include the following:
  • Boolean logic (AND, OR, XOR, NOT)
  • Comparative (greater than, less than, equal, not equal)
  • Mathematical (add, subtract, multiply, divide, average, negative)
  • Sequencers
  • Proportional-Integral-Derivative (PID) control
  • On or Off control