Wi-Fi - Facility Explorer - Part No. 24-10143-861 - Supervisory Device - FX Supervisory Controller

FX80 Supervisory Controller Installation Instructions

Product
Controls > Supervisory Controls > FX Supervisory Controller
Document number
Part No. 24-10143-861
Document revision
A
Revision date
2019-03-22

An integral Wi-Fi adapter provides wireless connectivity using the IEEE 802.11b/g/n standard, and provides an RP-SMA coax antenna connector.

The Wi-Fi configuration switch sets operation as follows:
  • OFF - (Default, middle) Wi-Fi adapter is disabled.
  • ACC - Controller provides operation as a Wi-Fi access point for up to 20 clients.
  • CLT - Controller operates as a client to an existing 802.11b/g/n router or access point.
Note: By default, the Wi-Fi software is disabled. You must enable the WiFi within the software before it becomes available.