An integral Wi-Fi adapter provides wireless connectivity using the IEEE 802.11b/g/n standard, and provides an RP-SMA coax antenna connector.
The Wi-Fi configuration switch sets operation as follows:
- OFF - (Default, middle) Wi-Fi adapter is disabled.
- ACC - Controller provides operation as a Wi-Fi access point for up to 20 clients.
- CLT - Controller operates as a client to an existing 802.11b/g/n router or access point.
Note: By default, the Wi-Fi software is disabled. You must enable the WiFi within the software before it becomes available.