Figure 1. Communications ports on the Controller

Callout |
Description |
---|---|
1 |
RS-485 ports and bias switches |
2 |
Wi-Fi adapter, settings switch, and antenna |
3 |
Ethernet ports, 10/100-Mbit, RJ-45 |
4 |
Earth ground and 24 V power input |