Remove or replace the microSD flash memory card - Facility Explorer - Part No. 24-10143-861 - Supervisory Device - FX Supervisory Controller

FX80 Supervisory Controller Installation Instructions

Product
Controls > Supervisory Controls > FX Supervisory Controller
Document number
Part No. 24-10143-861
Document revision
A
Revision date
2019-03-22

About this task

If necessary, you may need to remove or replace microSD flash memory card.

Figure 1. MicroSD card location in Controller

Table 1. MicroSD card location in Controller

Callout

Description

1

Access shutter for the microSD card (slide to open or close)

2

Card carrier inside the controller

3

MicroSD card to insert or remove from the card carrier

Important: Disconnect all power to the controller before removing or inserting the microSD card. Otherwise, equipment damage is likely to occur.
Note: When you remove the miscroSD card, you must lightly press on the installed microSD card shutter to release it. Then carefully remove the card from the card carrier. When you replace a microSD card, place the card in the card carrier, and push the card carrier in the access shutter until it clicks.
Note: Data on the microSD card is encrypted by a special system password stored in the controller base. If you are swapping in a card from a previously configured unit, you must re-enter this same passphrase using a serial connection to the unit’s debug port.
Note: Third-party microSD cards are not supported.