Mounting on the DIN rail - Facility Explorer - Part No. 24-10143-861 - Supervisory Device - FX Supervisory Controller

FX80 Supervisory Controller Installation Instructions

Product
Controls > Supervisory Controls > FX Supervisory Controller
Document number
Part No. 24-10143-861
Document revision
A
Revision date
2019-03-22

Procedure

  1. Pull the controller’s locking clip down.
    Figure 1. Fastening to the rail

  2. Tilt the module to hook over the DIN rail.
  3. Push down and in on the unit, fastening it to the rail.
  4. Slide the module firmly into the controller’s connector (or existing option module) to seat.
  5. Mount any option card module onto the DIN rail in the same way.
    Figure 2. Slide module into Controller's connector

  6. Slide the module firmly into the controller’s connector to seat. Repeat for other modules as needed (four maximum).
  7. Secure both ends of the final assembly with DIN rail end-clips provided by the DIN rail vendor.