The controller provides a number of status LEDs. All but one of the LEDs are visible with the front access door closed.
Figure 1. LEDs and descriptions

Callout |
Description |
---|---|
1 |
Wi-Fi (Green) - Lit when Wi-Fi configuration switch is not off |
2 |
RS-485 A (COM1) - Transmit (TX) and Receive (RX) |
3 |
RS-485 B (COM2) - Transmit (TX) and Receive (RX) |
4 |
STAT (Green) - Remains lit when controller is powered |
5 |
BEAT (Yellow) - Heartbeat, normally 1 Hz 50% duty cycle |
6 |
Secondary Ethernet - SEC (LAN2) Link and Activity |
7 |
Primary Ethernet - SEC (LAN1) Link and Activity |
8 |
(Behind door) BACKUP (Green) - Typically off |
If the BEAT LED stays on constantly, does not light, or blinks very fast, have your ABCS Distributor contact the FSC or your appropriate technical support group.
Important: The 1 Hz, 90/10 percent on/off BEAT flash at startup also occurs during other critical operations, such as a firmware upgrade to the controller or any attached modules. To be safe, do not remove power from the controller while its BEAT LED flashes with a 90/10 percent on/off duty cycle. Wait for the normal (50/50 percent) flash to return before removing power.