Parts included - Facility Explorer - Part No. 24-10143-861 - Supervisory Device - FX Supervisory Controller

FX80 Supervisory Controller Installation Instructions

Product
Controls > Supervisory Controls > FX Supervisory Controller
Document type
Installation Guide
Document number
Part No. 24-10143-861
Document revision
A
Revision date
2019-03-22
  • FX80 controller
  • MicroSD card installed in the controller
  • Coax-mount 2.4 GHz antenna for Wi-Fi, two 3-position RS-485 connector plugs, and a grounding wire
  • 2-position 24 VAC/DC connector plug
  • This FX80 Installation Sheet
  • FX80 IT Security Notice