Power wiring - Facility Explorer - Part No. 24-10174-115 - Supervisory Device - FX Supervisory Controller

FX30E/FX60E Supervisory Controllers Installation Instructions

Brand
Facility Explorer
Product name
FX Supervisory Controller
Document type
Installation Guide
Document number
Part No. 24-10174-115
Document revision
E
Revision date
2019-03-22
Language
English

The FX30E/FX60E must be powered by an approved 15 VDC power source. This source can come from one of the following:

  • a DIN rail mount 24 VAC/DC powered module (LP-FXPM24-0)
  • a DIN rail mount line voltage (120-240 VAC) module (LP-FXPM263-0)
  • an external Class 2 wall mount AC adapter (LP-FXPMUS/EU/UK-0)

The FX30E/FX60E does not include an on/off switch. To apply power, you can do one of the following:

  • plug in the power connector to the FX30E/FX60E, if the wall mount power module is used
  • plug in its 2-position power connector, if the 24 VAC DIN rail power supply is used
  • energize the AC circuit (120-240 VAC) wired to that module, if the line voltage DIN rail power supply is used
    CAUTION:
    • Risk of Property Damage.
    • Do not apply power to the system before checking all wiring connections. Short circuited or improperly connected wires may result in permanent damage to the equipment.
    CAUTION:
    • Risque dégâts matériels.
    • Ne pas mettre le système sous tension avant d'avoir vérifié tous les raccords de câblage. Des fils formant un court-circuit ou connectés de façon incorrecte risquent d'endommager irrémédiablement l'équipement.

If desired, you can use the wall mount power adapter in your office to initially commission the FX30E/FX60E, and then install the DIN rail mount power supply at the project site.

Important: Do not connect both the LP-FXPMUS and LP-FXPM24 supplies at the same time, or equipment damage may result.