Wiring the DIN rail mount line voltage power module - Facility Explorer - Part No. 24-10174-115 - Supervisory Device - FX Supervisory Controller

FX30E/FX60E Supervisory Controllers Installation Instructions

Brand
Facility Explorer
Product name
FX Supervisory Controller
Document type
Installation Guide
Document number
Part No. 24-10174-115
Document revision
E
Revision date
2019-03-22
Language
English

About this task

To wire the DIN rail mount line voltage power module, see Figure 1 and follow these instructions:

Procedure

  1. Remove power from the AC circuit being wired to the power module.
  2. Remove the power module cover by pressing in the four tabs on both ends of the unit, and lifting the cover off. If the power module is plugged into the FX30E/FX60E or an NDIO16, you may need to slide it away to access the cover tabs.
  3. Connect the supplied earth grounding wire to a nearby grounding point (Figure 8).
  4. Make AC circuit connections line (mains) and neutral to the terminals labeled INPUT PWR.
  5. Replace the cover on the power module.
  6. Make sure that all modules in the assembly are firmly connected together and secured.
    CAUTION:
    • Risk of Property Damage.
    • Do not apply power to the system before checking all wiring connections. Short circuited or improperly connected wires may result in permanent damage to the equipment.
    CAUTION:
    • Risque dégâts matériels.
    • Ne pas mettre le système sous tension avant d'avoir vérifié tous les raccords de câblage. Des fils formant un court-circuit ou connectés de façon incorrecte risquent d'endommager irrémédiablement l'équipement.