About this task
See Figure 1 to locate connectors and other components on the FX30E/FX60E. Make connections to the FX30E/FX60E in the following order.
Procedure
- Install any option cards (LON, RS-232, RS-485, modem, WTC) in Option Slots 1 and 2. See Mounting option cards for the general procedure. For complete details, refer to the specific mounting and wiring guide that shipped with the option card.
- Connect the supplied earth grounding wires (with spade connector) from the earth ground lug on the FX30E/FX60E and any accessory modules (if used) to a nearby earth grounding point. See Grounding for details.
- Prepare power wiring (leave the unit powered off). See Power wiring for details.
- Connect communications cables. See Communication wiring for ports available on the FX30E/FX60E base unit. For ports on any installed option card (LON, RS-232, RS-485, modem, and WTC), refer to the specific mounting and wiring guide for additional details.
- If NDIO modules are installed, connect the I/O wiring. Refer to the appropriate mounting and wiring guide for complete details.
- Apply power to the unit. See Powerup and initial checkout.