Using status LEDs - Facility Explorer - Part No. 24-10174-115 - Supervisory Device - FX Supervisory Controller

FX30E/FX60E Supervisory Controllers Installation Instructions

Brand
Facility Explorer
Product name
FX Supervisory Controller
Document type
Installation Guide
Document number
Part No. 24-10174-115
Document revision
E
Revision date
2019-03-22
Language
English

The FX30E/FX60E includes several LEDs that can help determine the status of the unit. These LEDs include:

  • Ethernet Ports
  • Heartbeat
  • Status
  • Serial Ports

See Figure 1 for the location of the status LEDs.